DLPU103B october 2020 – may 2023 DLP230NP
To begin, navigate to the base directory of the DLPDLCR230NPEVM python scripts and initialize the parallel video mode. Assuming that the python scripts have been loaded to:
/home/pi/Documents/dlp
Execute:
$ cd /home/pi/Documents/dlp
$ python3 init_parallel_mode.py
From here, display of any video content or images from the Raspberry Pi is possible. For example, at:
/home/pi/Documents/dlp/media
Navigate to the desired directory. It is recommended to use the list command to see what content is available:
$ ls -l
This folder is empty by default. To display video content, simply execute the following command (replace the file name with the desired video file):
$ omxplayer <filename>.mp4
The video will play in a letterbox by default. To stretch the video to play in fullscreen (regardless of the resolution) use the following command instead:
$ omxplayer --aspect-mode stretch <filename>.mp4
Press CTRL+C to exit the video playback.