Refer to Figure 4-11: DLPC964 System Block Diagram
DMDLOAD_REQ is an output signal from
the Apps FPGA to DLPC964 Controller.
Once an Aurora block data transfer is
completed, the Apps FPGA user logics must assert the DMDLOAD_REQ to signal the
DLPC964 that this is the end of a DMD block and trigger to carry out the operation
encoded in the Block Control word.
Guidelines for asserting the DMDLOAD_REQ signal and sending Block Control word:
- Apps FPGA user logics must wait
for the block transfer to be completed on all four Aurora data channels before
asserting DMDLOAD_REQ.
- Apps FPGA must take into
account that the four Aurora data channel interfaces are not fully
synchronous to each other, thus data completion do not happen at the
exact same clock cycle. Therefore, the Apps FPGA must monitor and verify
the Aurora block data transfer is completed on all four channels before
asserting DMDLOAD_REQ.
Note: Asserting DMDLOAD_REQ before completion of
Aurora block transfer can result in data not loaded properly to
DMD.
- DMDLOAD_REQ can be asserted immediately after completing an Aurora block
transfer, as long as the 300ns DMDLOAD_REQ setup time is met (refer to Section 4.3.3.11 for more information).
- Apps FPGA user logics must assert
DMDLOAD_REQ for the current block before initiate the transmission of the next
new DMD block. Every block must start with a Block Control word packet and end
with DMDLOAD_REQ assertion.
- DMDLOAD_REQ is still required for
operations that do not involve block data transfer (such as block clear/set
operation), and must still meet the 300ns setup time (refer to Section 4.3.3.11 for more information).
- Refer to Figure 4-19 for the scenario where after the Apps user
logics has completed the transfer of current block. The user can find that the
DLPC964 is still loading the previous block to the DMD (for example, BLKLOADZ is
low). The Apps FPGA can still assert the DMDLOAD_REQ while BLKLOADZ is low
because the DLPC964 can detect and store this DMDLOAD_REQ request. After
completing the Aurora data transfer of the current DMD block and asserting the
DMDLOAD_REQ signal, the Apps FPGA must wait for the de-assertion of BLKLOADZ by
the DLPC964 (for example, BLKLOADZ transition from low to high) before starting
the next block. De-assertion of BLKLOADZ means the DLPC964 has completed the DMD
data loading operation for previous block and a data buffer is freed up for
accepting a new data block from the Aurora interface.
Note: The DLPC964 has two data block buffers; one for
receiving the incoming Aurora data block, the other for holding the previous
block for streaming out to DMD. The buffers can be overrun and data is not
loaded correctly to the DMD if Apps FPGA does not synchronize the Aurora
block transfer with the BLKLOADZ’s de-assertion signal.
- Refer to Figure 4-20 for a scenario where the Apps FPGA chooses
to send the DLPC964 a DMD data block, but delay the assertion of the
DMDLOAD_REQ.
- Apps FPGA user logics assert
DMDLOAD_REQ immediately after the completion of current block data transmission
on all four Aurora data interfaces.
- DLPC964 de-assert BLKLOADZ indicating completion of data loading operation for
previous DMD block.
- Apps FPGA user logics detects the
de-assertion of BLKLOADZ and send a new Block Control word on Aurora channel 0
user-k port for next block.
- Apps FPGA user logics sending
data for the next block.
- BLKLOADZ asserted low by DLPC964
indicating that the data loading operation for the current block is triggered by
DMDLOAD_REQ.
- Apps FPGA finishes sending the
last block (block 15) data of current pattern and asserts DMDLOAD_REQ to
instruct the DLPC964 to carry out the data load operation.
- DLPC964 loading data to block 15
triggered by DMDLOAD_REQ from 1.
- Apps FPGA sends the first block
(block 0) of data of the next pattern over the Aurora data interfaces while the
DLPC964 is loading block 15 of the current pattern.
- DLPC964 de-asserts BLKLOADZ after
the data loading of block 15 of current pattern is complete. The Apps FPGA
detected the BLKLOADZ de-assertion as the last block of the current pattern and
has been loaded onto the DMD and issued a MCP_START for global block reset
operation.
- The Apps FPGA delayed the
assertion of DMDLOAD_REQ for block 0 for the next pattern due to the requirement
of meeting the mirror settling time.
- Send Block Control word for block
1 for the next pattern after the assertion of DMDLOAD_REQ for block 0.
- DLPC964 asserts BLKLOADZ to
indicate that the DMD data loading operation was triggered by DMDLOAD_REQ from
part 5.