DLPU133A March 2024 – February 2025 DLPC964
The signal integrity of the 10Gbps link can be verified with the Xilinx IBERT (Integrated Bit Error Ratio Tester) toolset. Refer to Xilinx user's guides (Section 6) for more details regarding the IBERT tool.
As shown in Table 4-1, there are four input ports to the RTL to control the TX transceiver setting. The TI EVM hardware are configured as below.
| Signal Name | I/O Direction | Clock Domain | Description |
|---|---|---|---|
| gt_txpostcursor_in[4:0] | Input | Async | Transceiver post-cursor TX pre-emphasis control. Set to "00000" for TI EVM hardware. Customers must perform IBERT eyescan to determine the best setting for the hardware. |
| gt_txdiffctrl_in[3:0] | Input | Async | Transceiver TX driver swing control. Set to "1000" (807mV differential peak to peak swing) for TI EVM hardware. Customer must perform IBERT eyescan to determine the best setting for the hardware. |
| gt_txmaincursor_in[6:0] | Input | Async | Transceiver main-cursor TX control. Set to "0000000" for TI EVM hardware. Customer musy perform IBERT eyescan to determine the best setting for the hardware. |
| gt_txprecursor_in[4:0] | Input | Async | Transceiver pre-cursor TX pre-emphasis control. Set to "00000" for TI EVM hardware. Customer must perform IBERT eyescan to determine the best setting for the hardware. |
In addition, the DLPC964 has an input pin RXLPEN to select between the low power mode (‘0’) or DFE (‘1’) equalization for the DLPC964 Xilinx GT cell transceiver. For TI EVM, RXLPEN is set to 0 for low power mode equalization. Refer to the Xilinx app note for information regarding RXLPEN.
With the above RX/TX transceiver settings (TX post-, main-, pre- cursor, TX diffctrl, and RXLPEN) selected and enabled in the IBERT GUI, Figure 4-27 shows an IBERT scan result of one of the 12 high speed links with eye opening of 200+ vertical codes, and 0.6UI horizontal at BER of 1e-12 (the purple area).
Figure 4-27 IBERT Eye-scan For Aurora
Channel0 Link0 Using TI EVM Hardware