- Block - A block is a 136
lines x 4096 pixels portion of the DMD. The DMD is split into 16 of these blocks
making the total image size of the DMD 2176 lines x 4096 pixels. Blocks can be
individually addressed (0x0 - 0xF) in the DLPC964 Apps FPGA.
- Segment - There are four
segments (A,B,C, and D) per block. Each segment consists of 136 lines x 1024
pixels. In normal operation, each of the 4 segments are loaded at the same time.
In slow mode each segment are loaded individually.
- Groups - When in double or
quad modes, blocks are updated in groups. These groups are outlined in the table
below. Note the importance that the user either enables all blocks in a group or
disabled all blocks in a group when in double or quad modes.
| Block Load Address |
0x0 |
0x1 |
0x2 |
0x3 |
0x4 |
0x5 |
0x6 |
0x7 |
0x8 |
0x9 |
0xA |
0xB |
0xC |
0xD |
0xE |
0xF |
| Double Mode Groups |
0x0 |
0x2 |
0x4 |
0x6 |
0x8 |
0xA |
0xC |
0xE |
| Quad Mode Groups |
0x0 |
0x4 |
0x8 |
0xC |
Below are simple timing examples of
sending blocks in x4 mode and global mode.
- DLPC964 Apps - The Xilinx
VC707 loaded with the Apps FPGA bitstream.
- DLPC964 - The DLPC964
Controller that interfaces with the DMD.
- Modes - There are 4 modes:
Single (0x0), Double or x2 (0x1), Quad or x4 (0x2), and Global (0x3). These
modes are explained in more detail below and in Section 3.
- Single (0x0) - In single
mode, each block is loaded with data and once the DLPC964 has finished loading
that individual block onto the DMD, the DMD is updated with the MCP_Start
signal. Since each block can be updated individually, the valid block mode
addresses are 0x0 - 0xF.
- Double (0x1) - Double mode
means that once the DLPC964 has loaded 2 blocks within a group with data, the
DMD updates both of these blocks with a single MCP_Start signal. Since 2 blocks
are updated at a time, the valid block mode address are 0x0, 0x2, 0x4, 0x6, 0x8,
0xA, 0xC, and 0xE.
Note: Note the importance to know that
when enabling and disabling blocks in double mode, all blocks within a group
must be enabled or disabled.
- Quad (0x2) - Quad mode
means that once the DLPC964 has loaded 4 blocks within a group with data, the
DMD updates all 4 blocks with a single MCP_Start signal. Since 4 blocks are
updated at a time, the valid block mode address are 0x0, 0x4, 0x8, and 0xC.
- Global (0x3) - This is the
default startup mode. In global mode, all enabled blocks are loaded and once the
DLPC964 has finished, the MCP_Start signal updates all the blocks at once. Since
all the blocks have been updated at once, the next load operation needs to wait
until the mirrors have settled.
Note: This is known as the
mirror settle time and must be around 8 us.
- Block Load Type - The
block load type is sent before the data using the user-k in the Aurora GTX
interface. The DMD supports 3 different types of loads; Normal (0x0), Clear
(0x1), and Set (0x2).
- Normal (0x0) - This is the
default block load type. The Normal load type tells the DLPC964 to load the DMD
with whatever data comes after the user-k data.
- Clear (0x1) - Clear load
type does not send any data. This is because when the DLPC964 receives a clear
load type, the DLPC964 sets the mirrors in the block specified to the off state
(0).
- Set (0x2) - Set load type
does not send any data. This is because when the DLPC964 receives the set load
type, the DLPC964 sets the mirrors in the block specified to the on start
(1).
- MCP_Start - The MCP_Start
(Mirror Clocking Pulse Start) signals the DMD to update the mirrors with
whatever data was sent. The DLPC964 determines which blocks to update based on
the Mode selected and the block mode address.
- Lines/Rows - A line of
pixels refers to the horizontal row of pixels 4096 across. Think of this as the
y-position on the DMD.
- Pixels/Columns - A column
of pixels refers to the vertical column of pixels 2176 across. Think of this as
the x-position on the DMD.
- Fast/Slow Mode - Fast mode
by default is enabled. Fast mode refers to sending all 4 segments of a block in
parallel across the 4 Aurora GTX channels. Slow mode uses only the first GTX
channel and sends the segments sequentially. Refer to the Pattern Modes section
for more details on the segment ordering.
- Load2 Mode - Load2 is
disabled by default. When in Load2 mode, the DLPC964 Apps only sends half of the
number of rows specified (136 lines requested, only 68 are sent). This is
because in this mode, the DMD loadS every 2 lines with the same data.