DLPU133A March 2024 – February 2025 DLPC964
The BRG (Block Reset Generator) module is a sub module of the BPG. The BRG is responsible for starting the PGEN (Pattern Generator) and interfacing with the DLPC964. There are several logic processes within the BRG to help determine when the time to start the PGEN and when to send another MCP_Start to the DLPC964 controller.
To keep the block diagram simple, the various processes within the BRG have been stated as Logic modules. Each of these logic modules are shown in the Figure 2-3 and explained in more detail below.
Figure 2-3 BRG Module Hardware Block Diagram