SBAA682 April 2025 AFE7728D , AFE7768D , AFE7769D
With the ideal condition of signal propogation from the MU to RU, the signal characteristic has a proper pulse filter to maintain the waveform meets various regional spectral mask requirements. If the signals go through typical Ethernet or fiber channel, the channel characteristic can introduce dispersion factor that can potentially widen the effective shape of the signal. In the case of repeater system, the signal goes through multi-path effect. In essence, the fiber dispersion factor and the repeater multi-path effect create a bandpass behavior and distorts the original pulse shaping filter. Therefore, to overcome the bandpass behavior, the design does the following: