SBAA682 April 2025 AFE7728D , AFE7768D , AFE7769D
An example of a typical wireless communications system environment using DAS is described in this section.
Figure 2-1 shows a typical service environment for DAS. Many private office buildings and public service buildings have many mobile users in a crowded and enclosed environment. The enclosed nature of the building environment does not allow external wireless signals from a base station (BTS) to reach inside the buildings. Therefore, without additional remedies to the wireless signal path, these buildings have coverage and capacity issues for the mobile users.
The building owners or manager can introduce DAS to simply redistribute the wireless signal path from outside the building to inside the building. Per Figure 2-2, a DAS typically consists of two principle elements: a master unit (MU) and one or more remote units (RU). The simplified operating principle is based on the master unit interface with an outside BTS or donor antenna that redistributes the outside signal indoors through indoor remote units. The indoor remote units can be placed throughout the building to improve coverage and capacity of the service. The key constraint is that the DAS is transparent to the mobile user and the BTS as the DAS is simply redistributing the signal.
The following summarizes the functionalities of each key component of the DAS:
New trend of the DAS design includes power distribution over Ethernet or over fiber. This approach allows the entire MU and RU to be powered over Ethernet or fiber line directly. The idea of power over cable is to allow the entire DAS system to be powered directly and independently from the main building power distribution service. The power utility bill can be separated between the DAS system and building owners.