SBAA702 July   2025 AFE8108 , AFE8190

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1 Introduction
  5. 2 Fast Bring-up on AFE81xx
  6. 3 Fast Bring-up Sequence
  7. 4 Input Parameter Constraint
  8. 5 Calibration Memory
  9. 6 Fuse Blow Requirement
  10. 7 Drifts and Aging
  11. 8 Device Bring-up Time
  12. 9 Summary
  13. 10References

Fast Bring-up Sequence

During first time bring-up, the result of the calibration is saved to the on-chip non-volatile (fuse) memory. Calibration Results are then loaded from fuse memory for subsequent bring-ups. Fuse blow is One-Time-Process, that is done during customer factory calibration when all system parameters are finalized. Faster bring-up time is achieved (368ms) at the cost of flexibility of input parameters.