SBAS710B September 2016 – April 2026 ADS9120
PRODUCTION DATA
In NAP mode, some of the internal blocks of the device power down to reduce power consumption in the ACQ state.
To enable NAP mode, set the NAP_EN bit in the PD_CNTL register. To exercise NAP mode, keep the CONVST pin high at the end of conversion process. The device then enters NAP mode at the end of conversion and continues in NAP mode until the CONVST pin is held high.
A CONVST falling edge brings the device out of NAP mode; however, the host controller can initiate a new conversion (CONVST rising edge) only after the tnap_wkup time has elapsed.
Figure 8-3 shows a typical conversion cycle with NAP mode enabled (NAP_EN = 1b).
Figure 8-3 NAP Enabled Conversion CycleThe cycle time is given by Equation 17.

At lower throughputs, cycle time (tcycle) increases but the conversion time (tconv) remains constant, and therefore the device spends more time in NAP mode, thus giving power scaling with throughput as shown in Figure 8-4.
Figure 8-4 Power Scaling with Throughput with NAP Mode