SBASAS5 October 2025 AMC0100R
PRODUCTION DATA
Place a minimum 10nF capacitor at the device input (from INP to INN). This capacitor helps avoid voltage droop at the input during the sampling period of the switched-capacitor input stage.
Do not short GND1 to INN directly at the device input. For best accuracy, route the ground connection as a separate trace that connects directly to the shunt resistor. See the Section 7.5.2 section for more details.
Do not leave the inputs of the AMC0100R unconnected (floating) when the device is powered up. If the device inputs are left floating, the device output is not valid.
Connect the high-side ground (GND1) to INN, either by a hard short or through a resistive path. A DC current path between INN and GND1 is required to define the input common-mode voltage. Do not exceed the input common-mode range specified in the Section 5.3 table.