To create a new platform in Vitis, follow these steps below:
- Open the File menu, go to New, and then click Platform Project (see Figure 8-1).
- Enter the desired platform name. The name ZCU102ps was used as an example (see Figure 8-2).
- After the new platform is named, a menu appears (see Figure 8-3). Select the XSA (Xilinx Support Archive) file.
- Browse and select the .XSA file from the FPGA folder shared along with this document (see Figure 8-4).
- Right-click the new platform project to open the drop-down menu. Click Build Project to start the build (see Figure 8-5). This can take some time to complete the build.