SBAU427 July 2025
Figure 2-3 shows all connections to the ADS131E08 (U1). Each analog power supply connection has a 1µF decoupling capacitor. Place these capacitors physically close to the device and make sure the capacitors have a good connection to the GND plane. Also, each digital input has a 10Ω series resistor. These resistors smooth the edges of the digital signals so that the signals have minimal overshoot and ringing. Although not strictly required, these components can be included in final designs to improve digital signal integrity.
The EVM uses the ADS131E08 internal clock by default. Alternatively, use an external clock by installing the JP1 header and then applying a clock signal to the CLK pin of JP1.