SBAU427 July 2025
Figure 4-6 shows the time domain display tool that allows visualization of the ADC response to a given input signal. This tool is useful for both studying the behavior and debugging any gross problems with the ADC or drive circuits. Capture the selected number of samples from the EVM by using the Capture button. The sample indices are on the x-axis while the y-axis shows the corresponding output codes or the equivalent analog voltages based on the specified reference voltage. Switching pages to any of the analysis tools described in the subsequent sections causes calculations to be performed on the same set of data.
Figure 4-6 Time Domain Display