SBOA643 October 2026 OPA591 , OPA596
The TINA-TI simulation results showing a maximum output power of approximately 22 W. Note that the output of the amplifier is significantly lower, consuming approximately 400mW of power, demonstrating the benefits of this circuit configuration. Select MOSFETs that have greater than 30W of power dissipation capability, such as FDD5N50, which has a power dissipation of at least 50 W. The maximum power dissipation at the output stage with a resistive load can be calculated using the following equation. Note that power consumption will vary with the load type (resistive vs. current). Refer to the TIPL on Power and Temperature for further details.
The value of RZCO can be iteratively determined through simulation. The results shown below demonstrate that resistor values below 100Ω cannot fully drive the loop. The 499 Ω resistor value drives 10.29mA of current, while the 1 kΩ drives 5.14 mA of current. The 1kΩ resistor has a thermal noise of approximately 4nV/√Hz, which is smaller than the op amp voltage noise of 13 nV/√Hz . Therefore, 1kΩ is a good choice for the RZCO, optimizing for both voltage noise and low power dissipation.
Given: R5 = 60.4 kΩ.
From the FDD5N50 datasheet, 3 V < VGS(th) < 5 V.
Optimize the resistor divider network by selecting R6 such that VGS(th) = 3 V.
Set VGS to nominal value 3 V to optimize for crossover distortion without cross conduction.
Choose conservative standard resistor value such that .
R6 and R7 can be further optimized for crossover distortion empirically, as individual VGS(th) values for the chosen MOSFET varies due to process variation.