SBOA643 October 2026 OPA591 , OPA596
OPA591 IHCP + Discrete Output Current Boost RZCO TINA
CircuitTINA simulations are run originally without the voltage divider as part of the circuit. This allows for insight into the optimized value of RZCO. Later, a voltage divider is added to the circuit to further optimize crossover distortion.
OPA591 Discrete Output Current Boost RZCO TINA Circuit
Simulation Results for RZCO and Corresponding IZCO
ValuesLooking at V_LOAD when RZCO = 1kΩ, there is still distortion. This distortion is due to the NMOS FET turning on. Adding a voltage divider to the circuit allows for a controlled VGS that is continuously applied to the gate of the MOSFET.
OPA591 IHCP + Discrete Output Current Boost Circuit TINA Circuit
OPA591 Discrete Output Current Boost Circuit Transient Simulation
ResultsThe post processor in TINA is used to calculate the average output power of the circuit (seen at node VOUT), using the same calculation as seen above in Equation 8.
OPA591 Discrete Output Current Boost Circuit DC Sweep Simulation
ResultsThe DC sweep analysis in TINA shows the linear relationship between the input voltage and the output current.