For best operational performance of the device, use good PCB layout practices, including:
- Noise can propagate into analog circuitry through the power pins of the circuit as a whole and op amp itself. Bypass capacitors are used to reduce the coupled noise by providing low-impedance power sources local to the analog circuitry.
- Connect low-ESR, 0.1µF ceramic bypass capacitors
between each supply pin and ground, placed as
close as possible to the device. A single bypass
capacitor from V+ to ground is applicable for
single-supply applications.
- Separate grounding for analog and digital portions of circuitry is one of the simplest and most-effective methods of noise suppression. One or more layers on multilayer PCBs are usually devoted to ground planes. A ground plane helps distribute heat and reduces EMI noise pickup. Make sure to physically separate digital and analog grounds paying attention to the flow of the ground current.
- To reduce parasitic coupling, run the input traces as far away as possible from the supply or output traces. If these traces cannot be kept separate, crossing the sensitive trace perpendicular is much better than in parallel with the noisy trace.
- Place the external components as close as
possible to the device. As illustrated in Figure 7-6, keep RF and RG close to the inverting input to minimize parasitic
capacitance.
- Keep the length of input traces as short as possible. Always remember that the input traces are the most sensitive part of the circuit.
- Consider a driven, low-impedance guard ring around the critical traces. A guard ring can significantly reduce leakage currents from nearby traces that are at different potentials.
- For best performance, clean the PCB following
board assembly.
- Any precision integrated circuit may experience
performance shifts due to moisture ingress into the plastic package.
Following any aqueous PCB cleaning process, bake the PCB assembly to
remove moisture introduced into the device packaging during the cleaning
process. A low-temperature, post-cleaning bake at 85°C for 30 minutes is
sufficient for most circumstances.