SBVA094A February   2025  – July 2025 TPS7A21

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Oscilloscope Basics
  5. 2Implications of Parasitics
  6. 3Common Oscilloscope Issues
    1. 3.1 Choosing an Oscilloscope Probe
    2. 3.2 Sufficient Sampling
    3. 3.3 Visualization
    4. 3.4 Measuring Currents Using Current Probes
    5. 3.5 Bandwidth Limiting and Averaging
  7. 4Parasitic Effects on Common Measurements
    1. 4.1 Load Transients
    2. 4.2 Power Supply Rejection Ratio
    3. 4.3 Output Noise Voltage
  8. 5Summary
  9. 6References
  10. 7Revision History

Measuring Currents Using Current Probes

Another common measurement for LDOs is to measure the input and output current using a current probe. Measuring current can be difficult to do with a current probe because the current probe requires that the current path is run through the probe. To accomplish this, sometimes a wire needs to be run out to create a loop around which the current probe can be connected, which introduces parasitic inductance. Any amount of parasitic inductance affects the shape of transient waveforms, and enough parasitic inductance can cause large resonant voltage spikes that distort the real behavior of the device. Load transient measurements were taken using the TPS793 device with a current probe which displays the output current on Channel 4 (green) in Figure 3-11. This load transient was collected with long cabling, which introduces significant parasitics. The additional parasitic inductance caused large resonant voltage spikes on the output of the device. Figure 3-12 shows a load transient measurement that includes significantly less cabling and minimal inductance, which leads to more accurate measurement data. Figure 3-12 shows the true device response to the load step, while Figure 3-11 does not.

 Current Probe Measurement
                        with Long CablingFigure 3-11 Current Probe Measurement with Long Cabling
 Current Probe Measurement
                        with Shortened CablingFigure 3-12 Current Probe Measurement with Shortened Cabling