SBVA094A February   2025  – July 2025 TPS7A21

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Oscilloscope Basics
  5. 2Implications of Parasitics
  6. 3Common Oscilloscope Issues
    1. 3.1 Choosing an Oscilloscope Probe
    2. 3.2 Sufficient Sampling
    3. 3.3 Visualization
    4. 3.4 Measuring Currents Using Current Probes
    5. 3.5 Bandwidth Limiting and Averaging
  7. 4Parasitic Effects on Common Measurements
    1. 4.1 Load Transients
    2. 4.2 Power Supply Rejection Ratio
    3. 4.3 Output Noise Voltage
  8. 5Summary
  9. 6References
  10. 7Revision History

Power Supply Rejection Ratio

Power Supply Rejection Ratio (PSRR) for LDOs is a measure of how well a small-signal ripple on the input is attenuated at the output. To learn more about PSRR and how to take a PSRR measurement, please see LDO PSRR Measurement Simplified.

In the following section, we review two PSRR measurement setup conditions taken with the TPS793 device, shown throughFigure 4-3. Condition one, shown with the red trace, shows a PSRR measurement taken with significantly longer cabling, while condition two, shown with the green trace, shows a PSRR measurement taken with significantly shorter cabling. When parasitics are introduced in a PSRR measurement, as shown with red trace, the PSRR measurement data collected at higher frequencies seems to be lower. At higher frequency measurements, especially for PSRR, the output capacitor characteristics significantly affects the measurement. With more parasitics tied to the output capacitor, the data collected at high frequencies shows the capacitor characteristics with those parasitics introduced.

 TPS793 PSRR with Additional
                    Parasitics Figure 4-3 TPS793 PSRR with Additional Parasitics