SCASE80 September 2025 TPUL2T323-Q1
PRODUCTION DATA
The TPUL2T323-Q1 is used to generate a fixed-width pulse from an input trigger event. This device is retriggerable, meaning that input triggers received while the output is active will cause the output pulse to extend and it will not expire until one configured time period after the most recent trigger.
The input trigger event comes from three gated inputs: T, T, and CLR. These inputs are combined in a 3-input AND gate, with T internally inverted such that the logic follows the boolean equation Y = !(T) • T • CLR. Each input has a Schmitt-trigger architecture, and thus includes hysteresis allowing for slow transitioning or noisy signals. An input signal is detected as a logic high if the signal is larger than VT+, and a low if the input signal is smaller than VT-. Between VT+ and VT-, the input signal is detected as the last valid state until one of those values is crossed. An output pulse is triggered on the rising edge of the aforementioned internal Y signal.
The output pulse width is controlled by the selection of external timing components Rext and Cext. Plots are provided in the Typical Characteristics section to easily select appropriate component values for a desired pulse width. See the Features section for additional information regarding the impact of external components on the timing accuracy of the TPUL2T323-Q1.