SCBA020A October 1999 – March 2020 TMS3705
This application report contains the following sections:
Section 2, Introduction: Gives a general description of the TIRIS™ system
Section 3, Key Features of the TMS3705: Outlines the key features of the TMS3705, a base station IC for TIRIS.
Section 4, Sequence Control: Provides general hints for initialization of the IC.
Section 5, Circuit Description of the Sample RF Module: Describes a sample circuit using the TMS3705A.
Section 6, Regulatory Notices and Ordering: Information on regulatory notices and ordering procedures.