SCDU033B February   2023  – November 2024

 

  1.   1
  2.   2
  3.   Trademarks
  4. Introduction
  5. General Texas Instruments High Voltage Evaluation Module (TI HV EVM) User Safety Guidelines
  6. Information About Cautions and Warnings
  7. Features
  8. TMUX9616QFPEVM GUI Software Installation
    1. 5.1 GUI Software Installation
    2. 5.2 GUI Software Quick Start Guide
  9. TMUX9616QFPEVM Setup Procedure
  10. TMUX9616QFPEVM Feature Descriptions
    1. 7.1 TX7516 Pulser Interface Headers
    2. 7.2 Thermal Shutdown
    3. 7.3 External SPI
    4. 7.4 Channel Loading Options
  11. Connection Descriptions
  12. Schematic
  13. 10Bill of Materials
  14. 11Revision History

General Texas Instruments High Voltage Evaluation Module (TI HV EVM) User Safety Guidelines

TMUX9616QFPEVM

Always follow TI’s setup and application instructions, including use of all interface components within their recommended electrical rated voltage and power limits. Always use electrical safety precautions to help ensure your personal safety and those working around you. Contact TI's Product Information Center http://support/ti./com for further information.

Save all warnings and instructions for future reference.

WARNING: Failure to follow warnings and instructions may result in personal injury, property damage, or death due to electrical shock and burn hazards.

The term TI HV EVM refers to an electronic product typically provided as an open framed, unenclosed printed circuit board assembly. It is intended strictly for use in development laboratory environments, solely for qualified professional users having training, expertise, and knowledge of electrical safety risks in development and application of high voltage electrical circuits. Any other use or application are strictly prohibited by Texas Instruments™. Unqualified professionals should immediately stop using the HV EVM.

  1. Work Area Safety
    1. Keep work area clean and orderly.
    2. One or more qualified observers must be present anytime circuits are energized.
    3. Effective barriers and signage indicating operation of accessible high voltages must be present in the area where the TI HV EVM and its interface electronics are energized for the purpose of protecting inadvertent access.
    4. All interface circuits, power supplies, evaluation modules, instruments, meters, scopes, and other related apparatus used in a development environment exceeding 50Vrms/75VDC must be electrically located within a protected Emergency Power Off EPO protected power strip.
    5. Use a stable and nonconductive work surface.
    6. Use adequately insulated clamps and wires to attach measurement probes and instruments. Do not test the EVM freehand whenever possible.
  2. Electrical Safety
    As a precautionary measure, it is always a good engineering practice to assume that the entire EVM may have fully accessible and active high voltages.
    1. De-energize the TI HV EVM and all its inputs, outputs, and electrical loads before performing any electrical or other diagnostic measurements. Revalidate that TI HV EVM power has been safely de-energized.
    2. With the EVM confirmed de-energized, proceed with the required electrical circuit configurations, wiring, measurement equipment connection, and other application needs, while still assuming the EVM circuit and measuring instruments are electrically live.
    3. After the EVM is completely ready, energize the EVM as intended.
    WARNING: While the EVM is energized, never touch the EVM or its electrical circuits, as they could be at high voltages capable of causing electrical shock hazard.
  3. Personal Safety
    1. Wear personal protective equipment (for example, latex gloves or safety glasses with side shields) or protect the EVM in an adequate lucent plastic box with interlocks to protect it from being accidentally touched.

Limitation for safe use:

Do not use the EVMs as all or part of a production unit.