SCDU033B February   2023  – November 2024

 

  1.   1
  2.   2
  3.   Trademarks
  4. 1 Introduction
  5. 2 General Texas Instruments High Voltage Evaluation Module (TI HV EVM) User Safety Guidelines
  6. 3 Information About Cautions and Warnings
  7. 4 Features
  8. 5 TMUX9616QFPEVM GUI Software Installation
    1. 5.1 GUI Software Installation
    2. 5.2 GUI Software Quick Start Guide
  9. 6 TMUX9616QFPEVM Setup Procedure
  10. 7 TMUX9616QFPEVM Feature Descriptions
    1. 7.1 TX7516 Pulser Interface Headers
    2. 7.2 Thermal Shutdown
    3. 7.3 External SPI
    4. 7.4 Channel Loading Options
  11. 8 Connection Descriptions
  12. 9 Schematic
  13. 10Bill of Materials
  14. 11Revision History

GUI Software Quick Start Guide

  1. Home Tab
    1. The Home Tab will display when launching the hardware software. Select the appropriate EVM GUI from the drop-down list that appears here. Press ‘connect’ after selecting the desired device for proper functionality.
    2. The Home tab will also contain the shortcut icon to the GUI in the Quick Start page.
TMUX9616QFPEVM TMUXHV-EVM GUI Home TabFigure 5-2 TMUXHV-EVM GUI Home Tab
  1. GUI Control Panel
    1. The GUI will provide control over the following pins and functionality:
      1. DIN – the 16 bits [D0:D15] are used to push data into the devices DIN pin. The ‘WRITE’ button will initialize the actual pushing of the bits starting with bit D15 as MSB.
      2. CLR – the CLR button will toggle the CLR GPIO input to the CLR pin on the device. The indicator light will be lit for a ‘high’ state and dimmed for ‘low’ state. The effects of this functionality can be found in the data sheet.
TMUX9616QFPEVM TMUXHV-EVM GUIFigure 5-3 TMUXHV-EVM GUI