SCDU035 December 2024
The TMUX2889YBHEVM has two 3-pin headers to control the power supply connection, location C2 of the TMUX2889, and the control inputs, location A2.
Header J2 connects the VDD pin to either the external power or to ground via a jumper. If Header J2 is not connected, then the devices supply is left floating. Figure 2-1 shows header J2.
Header J7 connects the SEL pin to either the external power or ground via a jumper. If Header J7 is not connected, then the devices SEL pin are left floating.
Figure 2-1 Header J2 : J2-1(GND), J2-2(Connection to device VDD), J2-3 (VDD_EXT)
Figure 2-2 Header J7 : J7-1(VDD_EXT), J7-2(Connection to device SEL), J7-3 (GND)The logic of headers J2(VDD) and J7(SEL) are shown at the top side of the TMUX2889YPHEVM.
Figure 2-3 TMUX2889YBHEVM Truth Table