SCEA154 July 2025 TXE8116 , TXE8116-Q1 , TXE8124 , TXE8124-Q1 , TXE8148
The current version of code composer studio can be downloaded from TI Developer Zone below the Common Actions section.
After downloading and opening the Code Composer Studio IDE, the example code can be found by browsing the software examples provided in the Resource Explorer.
Once the resource explorer is opened, follow the below directory to locate the sample code:
Arm^R-Based Microcontrollers → Embedded Software → MSPM0 SDK – 2.04.00.06 → Examples → Development Tools → LP-MSPM0C1104 LaunchPad → DriverLib → spi_controller_internal_loopback_poll → No RTOS → GCC Compiler → spi_controller_internal_loopback_poll
The sample project can be imported into the CCS IDE by clicking the 3 dots and selecting “Import to CCS IDE.”
Once imported, start by selecting the “spi_controller_internal_loopback_poll.syscfg” file.
The SPI settings in the example are to be modified through the SYSCONFIG GUI. Underneath SPI, select the following configurations to setup the code properly.
Figure 5-2 SYSCONFIG SetupSPI_0 is the name of the SPI peripheral in use. A custom profile is created. The mode is selected to be Controller with a target bit rate of 500kHz. Frame formatting is Motorola 4-wire SPI. Clock polarity set to LOW. Clock phase – data captured on first clock edge which is rising edge. Frame size is set to 8 bits. Bit order is MSB first. While chip select is CS0 – PA11, this example uses the GPIO on PA2 to capture the 3-byte framing structure for the TXE8124 device. CS0 – PA11 is ignored for this example.
Select the following for the Advanced Configuration tab making sure the Enable Internal Loopback is unchecked.
Figure 5-3 Below the Advanced
Configuration Tab, the Enable Internal Loopback is DisabledThe SYSCONFIG GUI sets up the SPI configuration without having to write code within the M0 driver library. This sets up the SPI driver giving more time to focus on the example functions for the TXE81XX.