SCEU029A August   2024  – December 2025

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Functional Blocks
      1. 2.1.1 Test Points
      2. 2.1.2 Programmer Header Block (P1)
      3. 2.1.3 External Connection Header Block
      4. 2.1.4 GPI Protection Block
      5. 2.1.5 I2C Address Block
      6. 2.1.6 Interface Select Block
      7. 2.1.7 RWS/RWB Socket
    2. 2.2 GPIO Testing Blocks
      1. 2.2.1 LED Blocks
      2. 2.2.2 Switch/LED Blocks
      3. 2.2.3 Switch Block
      4. 2.2.4 LED/Potentiometer Blocks
  9. 3Software
    1. 3.1 Using the TPLD1202-RWS-EVM
      1. 3.1.1 Equipment Needed for Programming
      2. 3.1.2 Installing Software
    2. 3.2 Configuring a TPLD Device
      1. 3.2.1 TPLD1202-RWS-EVM Setup for Programming
      2. 3.2.2 Inserting a TPLD1202RWS into the RWS/RWB Socket
      3. 3.2.3 Connecting the TPLD1202-RWB-EVM to a TPLD-PROGRAM Board
      4. 3.2.4 Temporarily Configuring a TPLD Device
      5. 3.2.5 Permanently Programming a TPLD Device
  10. 4Using the TPLD1202-RWS-EVM to Program TPLD1202RWB
  11. 5Hardware Design Files
    1. 5.1 Schematics
    2. 5.2 PCB Layout
      1. 5.2.1 PCB Overview
    3. 5.3 Bill of Materials
  12. 6Additional Information
    1. 6.1 Trademarks
  13. 7References
  14. 8Revision History

Programmer Header Block (P1)

The programmer header block accepts the 14-position cable used to connect the TPLD1202-RWS-EVM to the TPLD-PROGRAM. TI recommends using this header to connect only to the TPLD-PROGRAM using the cables included in the TPLD-PROGRAM kit. The header is keyed, so the 14-position cable can only be inserted to the case with the key facing the correct direction. To connect the TPLD1202-RWS-EVM to a TPLD-PROGRAM, follow the steps in Section 3.2.

SW4 connects the 3V3 line of the programmer header to the VCC line of the EVM. When powering the EVM from the TPLD-PROGRAM, the 3V3 line must be in the ON position.