SCEU029A August 2024 – December 2025
All cables included are keyed and can only be plugged in when facing the correct direction. If a cable cannot be inserted with the application of a gentle amount of force, try swapping the orientation of the cable and making sure that the header housings are unobstructed before trying again. Forcing the connections can cause damage to the cables and boards.
When the TPLD-PROGRAM is powered and connected the TPLD1202-RWS-EVM, LED1 and LED2 turns on if a shunt is placed on the associated jumpers. This is normal and is caused by I2C pull-ups installed on those lines on the TPLD-PROGRAM.
Figure 3-4 Keyed Header Socket