SDAA069 August 2025 TDA4VL-Q1
This application note explains how Linux based Dynamic Frequency Scaling (DFS) and the thermal management framework can be used on the TDA4VL device to manage CPU power and temperature effectively. The document highlights the current state of thermal sensor support, discusses DFS functionality, and provides guidance on integrating these features into embedded Linux systems.
The document also outlines an example implementation on the TDA4VL platform, showcasing how thermal CPU frequency scaling can be achieved using the Linux CPUFREQ and thermal frameworks.