SDAA099A September   2025  – October 2025 THS4531 , THS4531A , THS4535 , THS4541 , THS4551 , THS4561

 

  1.   1
  2. 12
  3.   Trademarks

Introduction

This application note aims to refine the process for converting a Multiple Feedback (MFB) filter for a traditional operational amplifier into a differential filter suitable for use with a fully differential amplifier (FDA). When using an FDA as an active filter, most online filter designers and tools simply do not include fully differential amplifiers in the analysis. There are multiple key benefits of utilizing a fully-differential amplifier to drive the inputs of these ADCs, including being able to convert single-ended signals into differential with DC coupling, adding gain and active filtration in one stage, independent output common mode control, improved second-order harmonic performance, and more.

For a more complete analysis of the various filter types (Butterworth, Bessel, and so on), transfer functions, supporting equations, and more, please consider evaluating the references listed at the end of this article.

MFB Operational Amplifier Implementation

At the simplest, an MFB filter can be designed for a traditional operational amplifier, and then simply flipped or mirrored onto the negative terminal and duplicated on both sides of the feedback network. To generate an op amp MFB model for conversion, use Texas Instrument's Filter Design Tool. Figure 1 demonstrates this principle with the core 5 basic components in the following.

 Operational Amplifier to Differential Amplifier MFB FilterFigure 1 Operational Amplifier to Differential Amplifier MFB Filter
Note: If the design being developed has a source impedance or requires a termination resistor, remember to add a resistor to the inverting input of the FDA to match the impedance of the non-inverting input. For more detailed information on this topic, please refer to the references at the end of this article.
 Differential Amplifier MFB Filter Driving an ADCFigure 2 Differential Amplifier MFB Filter Driving an ADC

Both capacitors labeled C2 can be combined in series into one passive component using equation (1) and as shown in Figure 6.

Equation 1. Ctotal=1C2+1C2=12C2

Simulation Implementation and Results

Table 1 outlines an example design requirement for one of the most common filter applications – an anti aliasing filter to drive a 1 MSPS SAR ADC. To generate the passive values, please use Texas Instrument's Filter Design Tool to generate an op amp filter that can be converted into an FDA filter.

Table 1 Design Requirements
Parameter Target Value
Filter Type 2nd Order Low Pass Butterworth (Q = 0.707)
Cut Off Frequency 500kHz
Target Gain 1V/V
FDA THS4535
ADC Sampling Rate 1MSPS
Target ADC ADS8860
 500kHz, Gain = 1V/V, Low Pass
                    Filter Schematic Figure 3 500kHz, Gain = 1V/V, Low Pass Filter Schematic
 500kHz, Gain = 1V/V, Low Pass
                    Filter OPA365 Op Amp Frequency Response Figure 4 500kHz, Gain = 1V/V, Low Pass Filter OPA365 Op Amp Frequency Response
 500kHz, Gain = 1V/V, Low Pass
                    Filter THS4535 FDA Frequency Response Figure 5 500kHz, Gain = 1V/V, Low Pass Filter THS4535 FDA Frequency Response

Table 2 outlines an additional design example with a gain of 2V/V to demonstrate single to differential conversion, addition of gain, and active filtration all while utilizing only one active component.

Table 2 Design Requirements
Parameter Target Value
Filter Type 2nd Order Low Pass Butterworth (Q = 0.707)
Cut Off Frequency 500kHz
Target Gain 2V/V
FDA THS4535
ADC Sampling Rate 1 MSPS
Target ADC ADS8860
 500kHz, Gain = 2V/V, Low Pass
                    Filter Schematic Figure 6 500kHz, Gain = 2V/V, Low Pass Filter Schematic
 500kHz, Gain = 2V/V, Low Pass
                    Filter OPA365 Op Amp Frequency Response Figure 7 500kHz, Gain = 2V/V, Low Pass Filter OPA365 Op Amp Frequency Response
 500kHz, Gain = 2V/V, Low Pass
                    Filter THS4535 FDA Frequency Response Figure 8 500kHz, Gain = 2V/V, Low Pass Filter THS4535 FDA Frequency Response

To further improve the filter matching and CMRR performance of your system, consider utilizing TI's precision matched resisters, RES11A.

Sallen-Key Implementation

Sallen-Key filters are not typically used with fully differential amplifiers, and therefore not considered in this document due to the dependency on a feedback path to both the inverting and noninverting terminal of a traditional op amp. In this configuration, the impedances on each terminal are mismatched – if this were to be replicated onto an FDA, the impedance mismatch would cause high distortion and other circuit abnormalities. Therefore, this is generally recommended to utilize an MFB filter topology as described previously for fully differential amplifiers.