SDAA111 October 2025 CC2340R5
The code projects supplied on the SimpleLink Low Power F3 Demos GitHub uses SimpleLink F3 SDK v9.11.0.18, SYSCONFIG Configuration Tool v1.22, and the TI CLANG v4.0.3 compiler. Please make sure that all of these dependencies are installed on your machine before attempting to import the project into Code Composer Studio (CCS) v20 or later. For more examples for setting up your environment, please refer to these SimpleLink Academy Labs: Resource Explorer. Please note that users are responsible for migrating and supporting any dependency versions not listed above.
Figure 3-1 CCS PropertiesTwo projects are included in the following