SDAA112 September 2025 AM625
In the peer file, the line
connect "/usr/sbin/chat -v -f /etc/ppp/peers/bg95-chat"
handles dialing and Packet Data Protocol (PDP) setup. If the AT commands fail, inspect the chat script closely for formatting issues.
For debugging, enable ECHO ON in the script, or run chat manually with the command below to watch the exchange without involving pppd.
chat -v -f script > /dev/ttyS0 < /dev/ttyS0
Note that stray or invisible characters in chat scripts can cause unexpected failures. Always edit in a plain text editor using UNIX line endings. Aborting conditions are strict: any matching abort string immediately stops the script. During experimentation, consider commenting out aborts to avoid premature exits.