SDAA112 September 2025 AM625
In many applications, a reliable gateway to the internet is necessary to enable communication, monitoring, or control of remote devices. Cellular modems provide an effective design when a traditional wired connection is not feasible, or when wireless (for example, 802.11) coverage is inconsistent. By leveraging PPP, a processor can seamlessly integrate a cellular modem as a network interface.
One significant application is in electric vehicle charging stations in dense urban environments. Building structures often attenuate or block Wi-Fi signals, limiting connectivity for payment processing or grid negotiation. Ethernet can be used in principle, but physical access to wired infrastructure is frequently restricted by security concerns or cost. A cellular modem provides an attractive alternative, offering a secure and dedicated path to the internet.
Building automation is another sector where PPP over cellular is useful. Many installations require coverage in remote corners of a facility where Wi-Fi cannot reach. Cellular connectivity provides a reliable and maintainable means of enabling communication without dependency on wired backhaul (e.g Ethernet or fiber optic cables). PPP is also widely adopted in transportation and logistics, where long-haul trucking and delivery fleets depend on cellular links to maintain reliable communication across wide geographic areas.