SDAA271 August   2026 LM339LV-Q1 , LM4060-Q1 , MSPM0G1507 , MSPM0G3218-Q1 , MSPM0G3507 , MSPM0G3519 , MSPM0L2117 , MSPM0L2228 , TPS388R0-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction to Functional Safety Voltage Monitoring requirements for MSPM0
  5. 2Functional Safety External Voltage Monitoring Recommendations
    1. 2.1 MSPM0 VCORE and VDD recommended requirements
    2. 2.2 Voltage Monitor Approaches
      1. 2.2.1 Voltage Supervisor - Multichannel Channel
      2. 2.2.2 Discrete Approach
  6. 3Summary
  7. 4References

MSPM0 VCORE and VDD recommended requirements

As mentioned in the safety mechanism regarding VCORE monitoring for the MSPM0 devices—using the MSPM0G3X0X and MSPM0GX51X devices as reference for the specific values used in this section —the following criteria must be fulfilled for the VCORE pin:
  • The voltage on the pin must be continuously monitored so that the system can detect both undervoltage (UV) and overvoltage (OV) conditions. The general considerations are as follows:

    • The VCORE pin can source up to 100 µA when operating in RUN or SLEEP mode (including while the device is held in reset). In STOP and STANDBY modes, the VCORE pin can source up to 20 µA. In SHUTDOWN mode the device is inactive, so no current can be sourced.
    • The VCORE pin cannot sink any current in any mode or at any point during the MCU’s operation.
The following VCORE values can be used as reference:
Table 2-1 VCORE Voltage Requirement Tables
VCORE recommended limits Min Typ Max Units Recommendation background
VCORE LDO Output Valid Limits 1.3 1.35 1.39 V The limits given are intended to prevent triggering any OV or UV condition as long as VCORE remains within these limits.
VCORE Absolute 1.27 1.42 V The limits given are intended to not be violated; otherwise, the device will go out of spec.
UV Threshold 1.27 1.285 1.3 V Allows for a margin of +/-1.17%
OV Threshold 1.39 1.405 1.42 V Allows for a margin of +/-1.07%
Note: The VCORE pin is physically present to provide access for a tank capacitor, which is part of the VCORE LDO circuit used to stabilize the VCORE voltage supplied to the internal circuits.
For system design purposes, the MSPM0 general guideline on VDD overvoltage is that the supply voltage should not exceed the recommended VDD maximum value (in this case, 3.6 V). Furthermore, the FTTI specifications for system fault detection and reaction must be defined by the designer, as they are dependent on the application.

The actions to take when a fault occurs depend on the application requirements. As mentioned in the specific device's safety manual, the actions that can be taken in the event of a fault range from communicating the error to a host CPU and allowing the system to take an appropriate action or resetting the MSPM0 device to ensure a "safe state" (in this context, this refers to setting the device to a state similar to reset, where pins and certain behaviors are set to a specific, known state).

Since a fault in VCORE can affect reset conditions in the MSPM0 device, it is required to consider only Power-On Reset (POR) as the default reset level the MSPM0 must undergo to be considered "reset." Furthermore, the voltage level at which the device is considered "powered off" must be at or below 0.9 V — the POR− device threshold — and this voltage level must be sustained for a period equal to or greater than 100 µs. Additionally, some of the potential failure modes resulting from a VCORE fault include the following:

  • Unkown state pins
  • Loss of the NRST mechanism
  • Loss of SRAM contents
  • Incomplete ongoing flash program/erase operations

Assuming the NRST is still valid (i.e. a VCORE fault is not ongoing), the following bench tested current consumption values can be used as a reference when the device is powered at the specified VDD levels while in the device is hold in reset:

  • Less than 20µA at VDD < 0.9V
  • Less than 30µA at VDD < 1.3V
  • Less than 700µA at VDD < 1.6V

Note: The currents above were measured while an MSPM0G3519 ran an empty project. Current values may vary depending on the application.