SDAA353 May 2026 TAS5802 , TAS5805M , TAS5815 , TAS5822M , TAS5825M , TAS5825P , TAS5827 , TAS5828M , TAS5830 , TAS5832
All TAS58xx devices have built-in over-current protection circuitry at the outputs. Each device will specify a typical over current protection threshold based on current capability of the internal clamp circuit. If the over-current threshold is exceeded the device will disable the Class-D output to avoid damage to the amplifier and the speaker. If an overcurrent event occurs, an overcurrent fault is reported at the corresponding register.