SDAA444 October 2026 UCC23711
The following figures show the schematic of the UCC23711 (U1) gate driver and the 1200V IGBT power module (Q1) used for testing and validation of the UCC23711.
Figure 3-2 IGBT Module and DC Bus SchematicA 1200V 6-pack IGBT power module Q1 in a 3-phase half bridge topology without a brake IGBT and with NTC was used. The IGBT module supports 25A continuous current and 50A peak current was used for the tests. The typical collector-emitter saturation voltage at 25°C is 1.6V at 15V across VGE and 25A current. The typical gate threshold voltage is 5.8V, the gate charge is 0.395µC at 600V and VGE=±15V, the internal gate resistor is typically 0Ω. When using a bipolar supply with 15V and -8V supply the corresponding gate charge is around 0.3µC, for a unipolar 15V supply is around 0.2µC. The gate charge impacts the bias supply power rating and decoupling caps. The turn-on delay time at 25°C is 35ns, the turn-off delay time is 190ns. This must be considered for the complementary PWM dead time setting.
In this design, the UCC23711 is selected due to the 6.5V DESAT threshold.