SFFS842A March   2024  – May 2025 TMCS1123-Q1 , TMCS1126-Q1 , TMCS1127-Q1 , TMCS1133-Q1

 

  1.   1
  2.   Trademarks
  3. 1Overview
  4. 2Functional Safety Failure In Time (FIT) Rates
  5. 3Failure Mode Distribution (FMD)
  6. 4Pin Failure Mode Analysis (Pin FMA)
    1. 4.1 TMCS1123-Q1 Pin FMA
    2. 4.2 TMCS1126-Q1 Pin FMA
    3. 4.3 TMCS1127-Q1 Pin FMA
    4. 4.4 TMCS1133-Q1 Pin FMA
  7. 5Revision History

TMCS1127-Q1 Pin FMA

This section provides a failure mode analysis (FMA) for the pins of the TMCS1127-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

Table 4-14 through Table 4-17 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Figure 4-3 shows the TMCS1127-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TMCS1127-Q1 data sheet.

TMCS1126-Q1 TMCS1133-Q1 TMCS1123-Q1 TMCS1127-Q1 TMCS1127-Q1 Pin Diagram Figure 4-3 TMCS1127-Q1 Pin Diagram

Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:

  • TA = -40°C to +125°C
  • VS = 3V to 5.5V
  • VCM = -1.3kV to 1.3kV
Table 4-10 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
IN+ 1 For forward current, hall-sensor bypassed, providing no signal to be sensed and amplified. If the IN+ pin is at a large potential above GND, this state results in a lot of current being sunk. Depending upon layout and configuration, this result can damage the input current system supply, the load device, or the actual device. A
IN- 2 For reverse current, hall-sensor bypassed, providing no signal to be sensed and amplified. If the IN- pin is at a large potential above GND, this state results in a lot of current being sunk. Depending upon layout and configuration, this result can damage the input current system supply, the load device, or the actual device. A
NC 3 Normal operation. D
VS 4 Power supply is shorted to ground. B
NC 5 Normal operation. D
VOUT 6 Output is pulled to GND and the output current is short circuit limited. When left in this configuration, while VS connected to a high-load-capable supply and for certain high-load conditions through the IN+ and IN- pins, the die temperature can approach or exceed 150°C. A
NC 7 Normal operation. D
NC 8 Normal operation. D
GND 9 Normal operation. D
NC 10 Normal operation. D
Table 4-11 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
IN+ 1 No current running through inputs. B
IN- 2 No current running through inputs. B
NC 3 Normal operation. D
VS 4 No power to the device. VOUT stays close to GND. B
NC 5 Normal operation. D
VOUT 6 Output is present at the pin, having no loading does not affect the output. However, the user sees unpredictable results further down on the signal chain. B
NC 7 Normal operation. D
NC 8 Normal operation. D
GND 9 GND is floating. Output is incorrect as the output is no longer referenced to GND. B
NC 10 Normal operation. D
Table 4-12 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effects Failure Effect Class
IN+ 1 IN- IN+ shorted to IN-. This creates a current divider which increases sensitivity error inversely proportional to the resistance of the short. C
IN- 2 NC If IN- > 6V, the device can be damaged. If NC is at VS and IN- < Vs, or if NC is at GND and IN- is at a large potential above ground, large current can be flowing between VS and the input current system supply. A
if IN- > 6V
B
otherwise
NC 3 VS Normal operation. D
VS 4 NC Normal operation. D
NC 5 VOUT Normal operation. D
VOUT 6 NC Normal operation. D
NC 7 NC Normal operation D
NC 8 GND Normal operation. D
GND 9 NC Normal operation. D
NC 10 IN+ If IN+ > 6V, the device can be damaged. If NC is at VS and IN+ < Vs, or if NC is at GND and IN+ is at a large potential above ground, large current can be flowing between VS and the input current system supply. A
if IN+ > 6V
B
otherwise
Table 4-13 Pin FMA for Device Pins Short-Circuited to supply
Pin Name Pin No. Description of Potential Failure Effects Failure Effect Class
IN+ 1 If IN+ > 6V, the device is damaged. If IN+ < Vs, a large amount of current can be pulled from VS. A
IN- 2 If IN- > 6V, the device is damaged. If IN- < Vs, a large amount of current can be pulled from VS. A
NC 3 Normal operation. D
VS 4 Normal operation. D
NC 5 Normal operation. NC
VOUT 6 The output is pulled to VS and the output current is short circuit limited. When left in this configuration, while VS is connected to a high-load-capable VS and for certain high-load conditions through the IN+ and IN- pins, the die temperature can approach or exceed 150°C. A
NC 7 Normal operation. D
NC 8 Normal operation. D
GND 9 VS is shorted to GND. B
NC 10 Normal operation. D