SLAA517F May 2012 – August 2021 MSP430F6720A , MSP430F6720A , MSP430F6721A , MSP430F6721A , MSP430F6723A , MSP430F6723A , MSP430F6724A , MSP430F6724A , MSP430F6725A , MSP430F6725A , MSP430F6726A , MSP430F6726A , MSP430F6730A , MSP430F6730A , MSP430F6731A , MSP430F6731A , MSP430F6733A , MSP430F6733A , MSP430F6734A , MSP430F6734A , MSP430F6735A , MSP430F6735A , MSP430F6736 , MSP430F6736 , MSP430F6736A , MSP430F6736A
The "source" folder structure is shown in Figure 5-4.
Figure 5-4 Source Folder StructureThe folder "emeter-ng" contains multiple project files. For this application, the emeter-6736.ewp project file is to be used. The folder "emeter-toolkit" has corresponding project file emeter-toolkit-6736.ewp. Choose only the projects that have the succeeding terms 6736 for this application. For first time use, it is recommended that both the projects be completely rebuild.
Figure 5-5 Toolkit Compilation in IAR
Figure 5-6 Metrology Project Build in IAR