SLAAE29 January   2023 MSPM0C1105 , MSPM0C1106 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3216 , MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Goals of Cybersecurity
    2. 1.2 Platform Security Enablers
  4. 2Device Security Model
    1. 2.1 Initial Conditions at Boot
    2. 2.2 Boot Configuration Routine (BCR)
    3. 2.3 Bootstrap Loader (BSL)
    4. 2.4 Boot Flow
    5. 2.5 User-Specified Security Policies
      1. 2.5.1 Boot Configuration Routine (BCR) Security Policies
        1. 2.5.1.1 Serial Wire Debug Related Policies
          1. 2.5.1.1.1 SWD Security Level 0
          2. 2.5.1.1.2 SWD Security Level 1
          3. 2.5.1.1.3 SWD Security Level 2
        2. 2.5.1.2 Bootstrap Loader (BSL) Enable/Disable Policy
        3. 2.5.1.3 Flash Memory Protection and Integrity Related Policies
          1. 2.5.1.3.1 Locking the Application (MAIN) Flash Memory
          2. 2.5.1.3.2 Locking the Configuration (NONMAIN) Flash Memory
          3. 2.5.1.3.3 Verifying Integrity of Application (MAIN) Flash Memory
      2. 2.5.2 Bootstrap Loader (BSL) Security Policies
        1. 2.5.2.1 BSL Access Password
        2. 2.5.2.2 BSL Read-out Policy
        3. 2.5.2.3 BSL Security Alert Policy
      3. 2.5.3 Configuration Data Error Resistance
        1. 2.5.3.1 CRC-Backed Configuration Data
        2. 2.5.3.2 16-bit Pattern Match for Critical Fields
  5. 3Secure Boot
    1. 3.1 Secure Boot Authentication Flow
    2. 3.2 Asymmetric vs. Symmetric Secure Boot
  6. 4Cryptographic Acceleration
    1. 4.1 Hardware AES Acceleration
      1. 4.1.1 Overview
      2. 4.1.2 AES Performance
    2. 4.2 Hardware True Random Number Generator (TRNG)
  7. 5Device Identity
  8. 6Summary
  9. 7References
  10. 8Revision History
  11.   A Security Enablers by Subfamily
Locking the Application (MAIN) Flash Memory

MSPM0 MCUs implement a static write protection scheme to lock out user defined sectors in the MAIN flash region from any program/erase operations at runtime. The desired static write protection scheme is configured as a part of the boot security policies in the NONMAIN flash region.

Purpose

Static write protection enables placement of a fixed, user-defined, application in the flash memory which has the following characteristics:

  • Once programmed and locked, it is not modifiable by the application code or ROM bootloader
  • If placed at the beginning of the flash memory, it is guaranteed to always be the first code which executes when the ROM boot configuration routine transfers execution to the user application

MSPM0 static write protection supports both characteristics, which must be satisfied to implement a secure boot image manager.

Capabilities

Any sector which is configured in the NONMAIN to be write-locked will be functionally immutable when the boot configuration routine transfers execution to either the bootstrap loader or the user application code in MAIN flash. Any attempt to program or erase a statically protected sector by the application code or the bootstrap loader will result in a hardware flash operation error, and the sector will not be modified.

While static write protection prevents any modification by application code or the boot loader, a mass erase or factory reset command sent through the SWD interface would be honored. If this behavior is not desired, the mass erase and/or factory reset SWD commands may be protected with unique passwords or disabled altogether (see the SWD policies). To completely remove any means of modifying statically write protected MAIN flash sectors, the mass erase and factory reset commands (or the SW-DP) must be disabled, and the NONMAIN boot configuration memory must also be statically write protected to prevent application code from changing the underling write protection scheme by modifying the contents NONMAIN region. This is discussed in the following section.