SLAAE56B November 2022 – August 2025 MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3105 , MSPM0G3106 , MSPM0G3107 , MSPM0G3505 , MSPM0G3506 , MSPM0G3507 , MSPM0H3216 , MSPM0L1105 , MSPM0L1106 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
The MSPM0 and STM32G0 both register and map interrupt and exception vectors depending on the device available peripherals. A summary and comparison of the interrupt vectors for each family of devices is included in Table 3-10. A lower value of priority for an interrupt or exception is given higher precedence over interrupts with a higher priority value. For some of these vectors the priority is user-selectable, and for others, this is fixed.
In the MSPM0 and STM32G0, exceptions such as NMI, reset, and hard fault handlers are given negative priority values to indicate that these always have the highest precedence over peripheral interrupts. For peripherals with selectable interrupt priorities, up to four programmable priority levels are available on both families of devices.
| NVIC Number | STM32G0 | MSPM0 | ||
|---|---|---|---|---|
| Interrupt/Exception | Priority | Interrupt/Exception | Priority | |
| - | Reset | Fixed: -3 | Reset | Fixed: -3 |
| - | NMI Handler | Fixed: -2 | NMI Handler | Fixed: -2 |
| - | Hard Fault Handler | Fixed: -1 | Hard Fault Handler | Fixed: -1 |
| - | SVCall Handler | Selectable | SVCall Handler | Selectable |
| - | PendSV | Selectable | PendSV | Selectable |
| - | SysTick | Selectable | SysTick | Selectable |
| 0 | Window Watchdog Interrupt | Selectable | INT_GROUP0: WWDT0/1, DEBUGSS, FLASHCTL, WUC FSUBx, and SYSCTL | Selectable |
| 1 | Power Voltage Detector Interrupt | Selectable | INT_GROUP1: GPIOA/B/C,
COMP0/1/2, TRNG(1) | Selectable |
| 2 | RTC and Timestamp | Selectable | TIMG8(1) | Selectable |
| 3 | Flash Global Interrupt | Selectable | UART3(1) | Selectable |
| 4 | RCC Global Interrupt | Selectable | ADC0 | Selectable |
| 5 | EXTI0 and EXTI1 interrupt | Selectable | ADC1(1) | Selectable |
| 6 | EXTI2 and EXTI3 interrupt | Selectable | CANFD0(1) | Selectable |
| 7 | EXTI4-EXTI15 interrupt | Selectable | DAC0(1) | Selectable |
| 8 | UCPD1/UCPD2/USB | Selectable | TIMG9(1) | Selectable |
| 9 | DMA1 Channel 1 | Selectable | SPI0 | Selectable |
| 10 | DMA1 Channel 2 and 3 | Selectable | SPI1(1) | Selectable |
| 11 | DMA1 Channel 4-6, and DMA2 Channel 1-5 | Selectable | SPI2(1) | Selectable |
| 12 | ADC and Comparator | Selectable | CANFD1(1) | Selectable |
| 13 | Timer 1 (TIM1), Break, Update, Trigger, and Commutation | Selectable | UART1(1) | Selectable |
| 14 | TIM1 Capture Compare | Selectable | UART4(1) | Selectable |
| 15 | TIM2 global interrupts | Selectable | UART0 | Selectable |
| 16 | TIM3 and TIM4 global interrupts | Selectable | TIMG0(1) | Selectable |
| 17 | TIM6, LPTIM1, and DAC interrupts | Selectable | TIMG6(1) | Selectable |
| 18 | TIM6 and LPTIM2 global interrupts | Selectable | TIMA0(1) | Selectable |
| 19 | TIM14 global interrupts | Selectable | TIMA1 | Selectable |
| 20 | TIM15 global interrupts | Selectable | TIMG7(1) | Selectable |
| 21 | TIM16 and FDCAN0 global interrupts | Selectable | TIMG12(1) | Selectable |
| 22 | TIM17 and FDCAN1 global interrupts | Selectable | TIMG14(1) | Selectable |
| 23 | 12C1 global interrupts | Selectable | UART5(1) | Selectable |
| 24 | I2C2 and I2C3 global interrupts | Selectable | I2C0 | Selectable |
| 25 | SPI1 global interrupts | Selectable | I2C1 | Selectable |
| 26 | SPI2 and SPI3 global interrupts | Selectable | I2C2(1) | Selectable |
| 27 | USART1 global interrupts | Selectable | UART7(1) | Selectable |
| 28 | USART2 and LPUART2 global interrupts | Selectable | AES(1) | Selectable |
| 29 | USART 3-6 and LPUART1 global interrupts | Selectable | UART6(1) | Selectable |
| 30 | CEC global interrupts | Selectable | RTC(1) | Selectable |
| 31 | AES and RNG global interrupts | Selectable | DMA | Selectable |
The MSPM0 devices include a dedicated event manager peripheral, which extends the concept of the NVIC to allow digital events from a peripheral to be transferred to the CPU as interrupts, to the DMA as a trigger, or to another peripheral to trigger a hardware action. The event manager can also perform handshaking with the power management and clock unit (PMCU), to make sure that the necessary clock and power domain are present for triggered event actions to take place.
In the MSPM0 event manager, the peripheral that generates the event is known as a publisher, and the peripheral, DMA, or CPU that acts based on the publisher is known as the subscriber. The potential combinations of available publisher and subscriber are extremely flexible and can be used when migrating software to replace functionality previously handled by interrupt vectors and the CPU, to bypass the CPU entirely. For example, an I2C-to-UART bridge can previously have triggered a UART transmission upon receipt of an I2C STOP, using an ISR to set a flag, or load the UART TX buffer directly. With the MSPM0 Event handler, the I2C transaction complete event can trigger the DMA to load the UART TX buffer directly, and therefore eliminate the need for any action by the CPU.
See the Events section of the MSPM0G technical reference manual or the MSPM0L technical reference manual to get more details on the use of the event handler in MSPM0.
Not to be confused with the MSPM0 event handler, the STM32G0 family of devices implement an extended interrupt and event controller (EXTI), which allows for the system wake from STOP mode through configurable events from IOs or peripherals. The wakeup features of the STM32G0 EXTI can be best replicated in MSPM0 using the IO wakeup features (see the IOMUX section of the MSPM0 technical reference manuals) and GPIO FastWake (see the GPIO section of the MSPM0 technical reference manuals). If the wakeup is for a single action, the Event handler peripheral is capable of requesting necessary PMCU resources for a peripheral operation to occur, and returning to the applicable low power mode after.