SLAAEF5B March 2024 – June 2025 MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G3506 , MSPM0G3507 , MSPM0H3215 , MSPM0H3216 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1
Here is the test based on a 3200mAh LiCO2 battery under 25°C. The u16MaxFullChgVoltThd setting is 4200mV. The EmptyDhgVoltThd setting is 3000mV.
Here is the test pattern:
Figure 5-7 Battery Test CaseAt the beginning, there is an obvious gap for NomSOC, CusSOC and SmoothSOC. See the test results in Figure 5-8. This is caused from first OCV calibration error.
The CusSOC has some gaps at the end of discharge, and this is because of EmptySOC. The SmoothSOC is flat and no jump at battery rest. All the data is controlled in the 0% to 100% range.
For different NomFullCap, the FltNomFullCap is updated after almost every rest. With the digital filter help, the NomFullCap gets more and more accurate. The MaxNomFullCap changes from 0 to a value, which means the output NomFullCap has an acceptable accuracy.
Figure 5-8 Battery Test ResultIf users want to check more parameters under debug mode with Q format, then right-click the value and select the related Q-Value format.
Figure 5-9 Read Q Values