SLAAEN2A February   2025  – August 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0C1105 , MSPM0C1105-Q1 , MSPM0C1106 , MSPM0C1106-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0G5115 , MSPM0G5116 , MSPM0G5117 , MSPM0H3215 , MSPM0H3215-Q1 , MSPM0H3216 , MSPM0H3216-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1116-Q1 , MSPM0L1117 , MSPM0L1117-Q1 , MSPM0L1126 , MSPM0L1126-Q1 , MSPM0L1127 , MSPM0L1127-Q1 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2116 , MSPM0L2117 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1

 

  1.   1
  2. 1Description
  3. 2Required Peripherals
  4. 3Design Steps
  5. 4Design Considerations
  6. 5Software Flow Chart
  7. 6Application Code
  8. 7Additional Resources
  9. 8Revision History
  10.   Trademarks

Design Steps

  1. Add the EEPROM emulation library. The MSPM0 software development kit (SDK) includes the EEPROM emulation library.
    Note: The EEPROM emulation library is based on the Flash API so the drivelib from SDK is also required.
    For Type A, the following files are needed:
    1. eeprom_emulation_type_a.c
    2. eeprom_emulation_type_a.h
    MSPM0L1306, MSPM0G3507, MSPM0C1104 EEPROM Emulation
                            Files Figure 3-1 EEPROM Emulation Files
  2. Add the include path in the code for eeprom_emulation_type_a.h. MSPM0L1306, MSPM0G3507, MSPM0C1104

    Users can modify the start address, the number of sectors to use, and the record size in eeprom_emulation_type_a.h. The default Flash address used for EEPROM emulation is 0x00001000, and 2 sectors are used by default, so 0x00001000-0x000017ff is occupied. Additionally, the default size of the emulated EEPROM is 128 bytes.

    1. #define EEPROM_EMULATION_ADDRESS (0x00001000)
    2. #define EEPROM_EMULATION_SECTOR_ACCOUNT (2)
    3. #define EEPROM_EMULATION_RECORD_SIZE (128)
  3. Define a global array as a buffer in random-access memory (RAM). Every time the system powers on, the data of the emulated EEPROM is loaded from Flash to this buffer using the initialize function. The size of array ought to be equal to the record size in step 2.
    • uint32_t EEPROMEmulationBuffer[EEPROM_EMULATION_DATA_SIZE / sizeof(uint32_t)];
  4. Add the initialize function at the beginning of main(), typically after SYSCFG_DL_init(). This action allows the relevant Flash areas to be formatted correctly and global variables to be allocated correctly. The initialize function EEPROM_TypeA_init() also searches the active record and loads the data from Flash to the buffer in step 3.
    • EEPROM_TypeA_init(&EEPROMEmulationBuffer[0]);
    MSPM0L1306, MSPM0G3507, MSPM0C1104 EEPROM
                            Initialization Figure 3-2 EEPROM Initialization
  5. Users can read or modify the buffer in RAM, as needed, after initialization. When the data from the buffer to Flash need to be stored, call EEPROM_TypeA_writeData() to create a new record in Flash.
    Note: After power down, the data in RAM is lost. To implement data storage after power loss, execute this function at least once.
    • EEPROM_TypeA_writeData(&EEPROMEmulationBuffer[0]);
    MSPM0L1306, MSPM0G3507, MSPM0C1104 EEPROM Write Figure 3-3 EEPROM Write
  6. Add the erase function according to the gEEPROMTypeAEraseFlag. Flash needs to be erased before writing data again and the smallest unit of erasure is sector. For EEPROM emulation, after one sector is full, gEEPROMTypeAEraseFlag is set. Users can call EEPROM_TypeA_eraseLastSector() according to the flag. For example, add the following code after EEPROM_TypeA_writeData() from step 5. Users can also choose an appropriate timepoint to erase the full sector, as needed.
    • EEPROM_TypeA_eraseLastSector();
    MSPM0L1306, MSPM0G3507, MSPM0C1104 EEPROM Erase Figure 3-4 EEPROM Erase

After steps 1 through 6, the EEPROM emulation Type A is implemented in the application. See Section 5 for the flow.