SLAAEN3A February   2025  – August 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0C1105 , MSPM0C1106 , MSPM0C1106-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3216 , MSPM0H3216-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1

 

  1.   1
  2. 1Description
  3. 2Required Peripherals
  4. 3Design Steps
  5. 4Design Considerations
  6. 5Software Flow Chart
  7. 6Application Code
  8. 7Additional Resources
  9. 8Revision History
  10.   Trademarks

Description

This subsystem demonstrates how to implement Electrically Erasable Programmable Read-Only Memory (EEPROM) emulation (Type B) in the application. EEPROM emulation allows a device to emulate EEPROM in Flash memory, and make an equivalent durability similar to EEPROM. The following features are available using Flash memory:

  • Data retention after unexpected power loss
  • Flexible structure for different applications
  • User-configured erase operation

Download the code for this example.

There are two types of EEPROM emulation libraries for MSPM0. Type A is to store one large block of data (64 bytes, 128 bytes or 256 bytes) with a Static Random Access Memory (SRAM) buffer. See the EEPROM Emulation Type A Design application note for details of the library. Type B is to store many small data items (16bit or 32bit) with item identifiers. See also the EEPROM Emulation Type B Design application note for details of the library.

This subsystem shows the usage of Type B. For the Type A subsystem, see the Emulate EEPROM With Flash (Type A) subsystem design.

Figure 1-1 shows a functional diagram of this subsystem.

MSPM0L1306, MSPM0G3507, MSPM0C1104 Subsystem Functional Block
                    Diagram Figure 1-1 Subsystem Functional Block Diagram