SLAAEO2 March   2025 AMC60704

 

  1.   1
  2.   Design Objective
  3.   Trademarks

Design Objective

Design a cost-effective, efficient, small, competitive circuit to consolidate AMC60704 power supply rails for biasing current output digital-to-analog converters (IDAC) and voltage output digital-to-analog converters (VDAC).

Input SupplyOperating RangeRecommended Device
MinimumMaximum
PVDD1.5V2.2VTPS62825A
VSS–5.5V–2.5VLM27761

Design Description

This circuit design creates a method to allow one main 3.3V power supply to supply multiple AMC60704 inputs. Important supplies are PVDD which supplies the IDAC that biases the lasers in an electro-absorption modulated laser (EML). Another important supply is VSS which is the input that supplies the VDAC in the negative range because VSS is used for biasing the electro-absorption modulator (EAM) in an EML.

Placing DC/DC converters on the PVDD and VSS rails allow the designers to provide a 3.3V supply and the converters step down and invert the input voltage to the desired value in range for PVDD and VSS. The suggested TPS6285A and LM27761 devices are small, low-cost, and efficient DC/DC converters that can step down and invert input voltages for PVDD and VSS. This design can be used in optical module applications for 400G. Additionally, 800G designs can be created but the 800G design requires an extra AMC60704 and LM27761 device.

AMC60704 Application Block DiagramApplication Block Diagram

Design Notes

  1. This design focuses on EML applications, thus VCC, the positive rail is grounded.
  2. This design can be used in 400G applications. Additionally, an 800G design can be created but the 800G design requires an extra AMC60704 and LM27761.
  3. For biasing the VDACs in an EML application, the operating range for the VSS is rail is –2.5V to –5.5V. This circuit design uses –3.3V to supply the VDACs.
  4. The AMC60704 has four VDAC channels each capable of a 50mA output. In 400G applications, all 4 channels are used. This circuit design uses all four VDAC channels.
  5. The LM27761 has a maximum output current of 250mA and a configurable output range of –1.5V to –5V making the device a good fit for the VSS rail. The following image shows a typical LM27761 schematic.
    AMC60704 LM27761LM27761
  6. The output voltage of the LM27761 is externally configurable. The values of R1 and R2 determine the output voltage setting. Use Equation to calculate the output voltage. The value for R2 must be no less than 50kΩ.
    VOUT=-1.22V×(R1+R2R1)
    • This design operates at –2.85V VSS, thus R1= 30.1kΩ and R2 = 39kΩ, to allow enough headroom for current sourcing.
  7. Different output capacitance values can be used to reduce charge pump ripple, shrink the design size, or cut the cost of the design. In typical applications, a 4.7µF low-ESR ceramic charge-pump output capacitor (C3) is recommended.
  8. Increasing the input capacitance results in a proportional decrease in input voltage ripple. Input voltage, output current, and flying capacitance also affect input ripple levels to some degree. A 4.7µF low-ESR ceramic capacitor is recommended on the input.
  9. Flying capacitance can impact both output current capability and ripple magnitudes. In typical high-current applications, 0.47µF or 1µF 10V low-ESR ceramic capacitors are recommended for the flying capacitors.
  10. The LDO output capacitor (C4) value and the ESR affect stability, output ripple, output noise, PSRR and transient response. The LM27761 only requires the use of a 2.2µF ceramic output capacitor for stable operation.
  11. For biasing the IDACs in an EML application, the operating range for the PVDD rail is 1.5V to 2.2V. This circuit design uses 1.8V to supply the IDACs.
  12. The AMC6V704 has four IDAC channels each with a 200mA full scale output. The maximum output current for the IDACs is 800mA.
  13. The TPS62825A is selected for this design because the device has a maximum output current of 2A and adjustable output voltage range from 0.6V to 4V. These converters maintain a continuous conduction mode operation and keep the output voltage ripple very low across the whole load range. The following image shows a typical TPS62825A schematic.
    AMC60704 TPS62825A SchematicTPS62825A Schematic
  14. Use the following equation to set the output voltage on the TPS62825A.
    R1=R2×(VOUTVFB-1)
    where
    • VFB is 0.6V
  15. R2 must not be greater than 100kΩ to achieve high efficiency at light load while providing acceptable noise sensitivity. The following equation shows how to compute the value of the feedforward capacitor, C3 for a given R2 value. For the recommended 100kΩ value for R2, a 120pF feedforward capacitor is used.
    C3=12μR2
  16. Considering the DC-bias derating the capacitance, the minimum effective output capacitance, C2, is 10µF for the TPS62825A.
  17. A minimum effective input capacitance, C1, of 3µF must be present, though a larger value reduces input current ripple. A 4.7µF input capacitor is used for the TPS62825A.
  18. Adding the TPS62825A to the system, the power dissipation of the IDACs is now a function of the TPS62825A output voltage and current output, PVDD supply voltage, the current output, and the voltage of the IDAC pin. The power dissipation is calculated using this equation. The VHEADROOM voltage is calculated as the difference between PVDD and VIDACx.
    AMC60704 PVDD Power DissipationPVDD Power Dissipation
  19. PTPS62825A=3.3V×I3_3-[PVDD×IOUT+PVDD×IQPVDD+∑IDAC0-3VHEADROOM×IDACx]
    1. The power dissipation can be reduced by minimizing the voltage difference, VHEADROOM, between PVDD supply and VIDAC. The minimum PVDD is 1.5V.
    2. The output load can be calculated using the following equation.
      LOAD=VIDACIDAC
  20. Package Size Comparison shows the products used in this design. Selecting the key passive components was previously discussed. For more complete details, see the product data sheet. A key requirement for this design is small package size due to high channel density within an optical module. The following image shows the package size comparison.
    AMC60704 Package Size ComparisonPackage Size Comparison
  21. To compete in this market, this design creates a low-cost answer against integrated devices.

Design Measurements

Test 1: Power Supply Ramp-Up Response

Power Supply Ramp-Up Response shows the power supply ramp-up response test setup and test points.

AMC60704 Power Supply Ramp-Up ResponsePower Supply Ramp-Up Response

The Power Supply Ramp-Up Response graph shows the time required after a power-on trigger occurs for the power supplies in the system to respond. The Tektronix TBS 2000B oscilloscope was used to probe each power supply input to measure the ramp-up for this test.

AMC60704 Power Supply Ramp-Up ResponsePower Supply Ramp-Up Response

Test 2: Power Efficiency of System vs IDAC

This efficiency test measures the power dissipation at the input supply of the TPS62825A against the power dissipation of the IDAC with a 4.99Ω load. As the IDAC codes change, the output of the IDAC as well as the input power changes. IDAC Test Setup shows the setup for this test.

AMC60704 IDAC Test SetupIDAC Test Setup
AMC60704 IDAC Efficiency vs IDAC OutputIDAC Efficiency vs IDAC Output
AMC60704 IDAC Power vs IDAC OutputIDAC Power vs IDAC Output
AMC60704 IDAC System Power vs IDAC OutputIDAC System Power vs IDAC Output

Test 3: Power Efficiency of System vs VDAC

This test shows the power dissipation of the input supply from the LM27761 and the output of the VDAC. The following image shows the setup and test points. Using a DMM in a current measurement configuration, measuring the input current of the LM27761 can be used to calculate the power of the system. By changing the VDAC codes, the output of the VDAC changes as well as the system current. Placing a load resistor at the output allows for the calculation of the current flowing through the load. For a maximum output current of 50mA at full scale voltage output of –2.5V, the maximum resistive load is 50Ω.

AMC60704 VDAC Test SetupVDAC Test Setup
AMC60704 VDAC Efficiency vs VDAC Current Drive OutputVDAC Efficiency vs VDAC Current Drive Output
AMC60704 VDAC System Power vs VDAC Current Drive OutputVDAC System Power vs VDAC Current Drive Output
AMC60704 VDAC System Power vs Load PowerVDAC System Power vs Load Power

Design Featured Devices

DeviceKey FeaturesLinkOther Possible Devices
AMC6V704Optical controller with four 200mA current DACs, four voltage-output DACs and a multichannel ADCAMC6V704AMC60704
TPS62825A2.4V to 5.5V input, 2A step-down converter with forced PWM in 1.5mm × 1.5mm VSON-HR packageTPS62825ATPSM82822
LM27761Low-noise regulated inverter with integrated LDO for an input voltage in the range of 2.7V to 5.5VLM27761LM27762