SLAAEO4 November 2025 MSPM0G3507 , MSPM0L1306
The alert feature is applied in ROM BSL for cases where there are occurrences of more than 3 incorrect BSL password checks. By default, the device does not perform additional actions when a security alert is raised. User can configure the alert behavior through the BSLCONFIG2.ALERTACTION field.
In the BSL configuration, two additional alert behaviors are supported:
Set the flash memory static write protection (Section 3.1.3) to retain specific MAIN flash memories or the entire NONMAIN flash memory.