SLAAEQ5 March 2025 MSPM0C1103 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0C1105 , MSPM0C1106 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3215 , MSPM0H3216 , MSPM0L1105 , MSPM0L1106 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2228 , MSPM0L2228-Q1
Based on cybersecurity, automobile manufacturers put forward the following requirements for MCU chips:
Based on this requirement, commonly-used automotive MCUs have integrated hardware to support changing the debug access mode to the encryption mode. The G and L series of MSPM0 has the BOOTCFG0 register to support that.
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | SWDP_MODE | R/W | AABBh | The serial wire debug port (SW-DP) access policy. This
policy sets whether any communication is allowed with the device via
the SWD pins (to any DAP). When disabled, no SWD communication is
possible regardless of the configuration of the DEBUGACCESS field.
5566h = The SW-DP is fully disabled and no device access is possible via the SW-DP (0x5566 and all other values NOT 0xAABB). AABBh = The SW-DP is enabled and device access is set by the additional policies in NONMAIN. |
| 15-0 | DEBUGACCESS | W | AABBh | The debug access policy for accessing the AHB-AP,
ET-AP, and PWR-AP debug access ports. Note that if SWDP_MODE is set
to DISABLED, then the value of this field is ignored and the debug
port remains fully locked. 5566h = Access to AHB-AP, ET-AP, and PWR-AP via SWD is disabled (0x5566 and all other values NOT 0xCCDD or 0xAABB). AABBh = Access to AHB-AP, ET-AP, and PWR-AP via SWD is enabled. CCDDh = Access to AHB-AP, ET-AP, and PWR-AP via SWD is only enabled when the correct password is provided via the DSSM before BCR execution. |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | SWDP_MODE | R/W | AABBh | The serial wire debug port (SW-DP) access policy. This
policy sets whether any communication is allowed with the device via
the SWD pins (to any DAP). When disabled, no SWD communication is
possible regardless of the configuration of the DEBUGACCESS field.
AABBh = Enabled; FFFFh = Disabled (all other values). |
| 15-0 | DEBUGACCESS | W | AABBh | The debug access policy for accessing the AHB-AP,
ET-AP, and PWR-AP debug access ports. Note that if SWDP_MODE is set
to DISABLED, then the value of this field is ignored and the debug
port remains fully locked. AABBh = Access to AHB-AP, ET-AP, and PWR-AP via SWD is enabled; FFFFh = Access to AHB-AP, ET-AP, and PWR-AP via SWD is disabled (all other values). |
However, for some low-cost MCU like MSPM0 C series, this function is cut off because of cost. This application note explains how to implement encryption debugging through software to make this type of MCU without hardware support also meet the cybersecurity requirements.
Also, not only C but L and G series can also use this software method for a more flexible application.