SLAAER8 August 2025 MSPM0C1104 , MSPM0G1106 , MSPM0G1107 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0L1306
To change the watchdog timer period and the reset pulse length easily, modify the #defines in watchdog_hal.h, as demonstrated in the following code block:
#ifndef WATCHDOG_FUNCTION_H_
#define WATCHDOG_FUNCTION_H_
#include"ti_msp_dl_config.h"
#define WATCHDOG_1s (32768)
#define WATCHDOG_500ms (WATCHDOG_1s/2)
#define WATCHDOG_250ms (WATCHDOG_1s/4)
#define WATCHDOG_125ms (WATCHDOG_1s/8)
#define WATCHDOG_100ms (WATCHDOG_1s/10)
#define WATCHDOG_50ms (WATCHDOG_1s/20)
#define WATCHDOG_25ms (WATCHDOG_1s/40)
#define WATCHDOG_12D5ms (WATCHDOG_1s/80)
#define WATCHDOG_10ms (WATCHDOG_1s/100)
#define delay_1s (24000000)
#define delay_20ms (delay_1s/50)
#define delay_10ms (delay_20ms/2)
#define delay_5ms (delay_20ms/4)
#define delay_2D5ms (delay_20ms/8)
#define delay_2ms (delay_20ms/10)
/* User defined */
#define WATCHDOG_PERIOD (WATCHDOG_1s)
#define WDO_RESET_TIME (delay_10ms)
void watchdog_start(void);
void watchdog_timeout(void);
void watchdog_reload(void);
#endif /* WATCHDOG_FUNCTION_H_ */