SLAAEV0 July 2026 BQ79616-Q1
To achieve the reverse wake-up function, the OVUVOTUT function needs to be configured before the BQ79616 enters Sleep mode, so as to implement its monitoring of battery pack voltage and temperature in Sleep mode. After entering Sleep mode, other modules are deactivated, and only the OVUVOTUT module and communication module continue to operate. The power consumption of the chip in Sleep mode primarily includes the power consumption of the protection module and the communication module.
The implementation logic for the OVUV function of the BQ79616 is shown in the figure below. After configuring the OVUV thresholds via registers, the chip's OVUV DAC generates the corresponding analog voltages to the input terminals of the comparators. The other terminal of the comparator is connected to the cell voltage through a MUX and a BCI shifter. When a cell voltage exceeds the configured threshold, the OVUV fault is asserted.
By the same token, the implementation logic for the OTUT function is shown in the figure below. The divided voltage between the pull-up resistor and the NTC sampled by the GPIO port is compared against the OTUT threshold via a comparator. An OTUT fault bit is asserted after an OTUT event occurs. The OTUT thresholds are configured in terms of percentage. A threshold percentage configuration of 50% means that after the NTC resistance (thermistor) at a certain temperature divides the voltage with the pull-up resistors (R1, R2), the voltage input to the GPIO equals 50% of the TSREF voltage.
The registers relevant to the OVUVOTUT configuration include:
In Sleep mode, the BQ79616 performs real-time periodic checks for OVUVOTUT, OTCB, and CBDONE. As shown in Figure 1-5, the OV check and UV check are carried out simultaneously. The difference lies in that the VCB_DONE balancing end-of-voltage check is interspersed within the UV check. As shown in Figure 1-6, the OT check and UT check are also conducted alternately, and OTCB balancing overtemperature is interspersed within the OT sequence.
During the diagnostic process, if any fault among OVUVOTUT is monitored, the BQ79616 will transmit a fault tone to the BQ79600, and the BQ79600 reverse-wakes the MCU.
Figure 1-5 Operation Timing of BQ79616 OVUV/CBDONE in Sleep Mode
Figure 1-6 Operation Timing of BQ79616 OTUT/OTCB in Sleep Mode