SLAU319AF July 2010 – September 2022
Simple CMOS inverters with Schmitt-trigger characteristics (IC2) are used to transform the RS-232 levels (see Table 4-2) to CMOS levels.
| Logic Level | RS-232 Level | RS-232 Voltage Level |
|---|---|---|
| 1 | Mark | –3 V to –15 V |
| 0 | Space | 3 V to 15 V |
The inverters are powered by the operational amplifier IC3A. This amplifier permits adjusting the provided logic level to the requirements of the connected target application. A voltage applied to pin 8 of the BSL target connector (VCC_IN) overrides the default 3-V level provided from IC1 and the 100-kΩ series resistor R11. Thus, the output voltage of the operational amplifier is pulled to the applied voltage VCC_IN.
Depending on the overvoltage protection of the device family selected, the excess voltage is either conducted to VCC (as in the TI 74HC14) or to GND (as in the TI 74AHC14). If the protection diode conducts to VCC, the operational amplifier IC3A needs to compensate for the overvoltage. Therefore, TI recommends the 74AHC14 device, which conducts to ground (GND).
To avoid excessive power dissipation and damage of the protection diodes, series resistors (R1, R2, and R3) are used to limit the input current.
An operational amplifier (IC3B) is used to generate RS-232 levels out of CMOS levels. The level at the positive input is set to VCC/2 (1.5 V nominal). If the level at the negative input rises above this level, the output is pulled to the negative supply of the operational amplifier (mark). If the level drops below VCC/2, the output is pulled to the positive rail (space).
The positive supply of the operational amplifier is the same as the input to the voltage regulator. A separate capacitor (C5) is used to generate the negative supply voltage. This capacitor is charged by the receiving signal of the bootloader hardware (pin 3 on SUB-D connector J2).
During an asynchronous serial communication, the combination of stop bit and start bit is used to synchronize sender and receiver. After the transmission of a data byte, the stop bit forces the transmission line into a defined state, which is usually a logic 1 or, in RS-232 terms, a mark. This means that the transmission-line voltage is negative when there is no transmission and the capacitor can be charged. Diodes are used to prevent discharge of the capacitor during transmission.
In very rare circumstances, the data sent to the bootloader interface might hold too many zeros, so that the capacitor C5 required for the negative supply is discharged, causing a malfunction of the interface. (A possible workaround is to send the data in smaller chunks.) However, under normal operating conditions, even data that contains all zeros does not cause problems.