SLAU319AF July 2010 – September 2022
The Peripheral Interface for the USB bootloader has the wrapper format shown in Table 3-4. There are no interface specific commands or replies for the USB BSL. The only variable byte, NL, should describe the number of bytes contained in the BSL Core Command packet.
| Header | Length | BSL Core Command |
|---|---|---|
| 0x3F | NL | See Section 3.5 |