SLAU599B August 2015 – July 2021
Five software examples are included with the MSP-EXP432P401R LaunchPad development kit for the Educational BoosterPack plug-in module MKII (see Table 3-1). These examples can be found in the MSP-EXP432P401R Software Examples, or they are more easily accessible through the SimpleLink MSP432™ software development kit (SDK) (see Section 4.3).
| Demo Name | LaunchPad Development Kit / BoosterPack Plug-in Module Required | Description | More Details |
|---|---|---|---|
| BOOSTXL-EDUMKII_ Accelerometer_MSP432P401R | MSP-EXP432P401R / BOOSTXL-EDUMKII | Demonstrates how to sample data from the analog accelerometer sensor using the MSP432 ADC14 | Section 3.1 |
| BOOSTXL-EDUMKII_ JoyStick_MSP432P401R | MSP-EXP432P401R / BOOSTXL-EDUMKII | Demonstrates how to sample data from the analog joystick using the MSP432 ADC14 | Section 3.2 |
| BOOSTXL-EDUMKII_ LightSensor_MSP432P401R | MSP-EXP432P401R / BOOSTXL-EDUMKII | Demonstrates how to communicate with the digital ambient light sensor through I2C using MSP432 | Section 3.3 |
| BOOSTXL-EDUMKII_ Temperature_MSP432P401R | MSP-EXP432P401R / BOOSTXL-EDUMKII | Demonstrates how to communicate with the digital temperature sensor through I2C using MSP432 | Section 3.4 |
| BOOSTXL-EDUMKII_ MicrophoneFFT_MSP432P401R | MSP-EXP432P401R / BOOSTXL-EDUMKII | Demonstrates how to sample audio and perform FFT using the ARM CMSIS DSP Software Library | Section 3.5 |
To use any of the software examples with the LaunchPad development kit, you must have an integrated development environment (IDE) that supports the MSP432P401R device (see Table 3-2). For more details on how to get started quickly, and where to download the latest Code Composer Studio, IAR, and Keil IDEs, see Section 4.
| Code Composer Studio™ IDE | IAR Embedded Workbench® IDE | Keil®µVision® MDK-ARM |
|---|---|---|
| v7.1.0 | v7.80.3 | v5 |