Follow the steps below when connecting
an MSPM0 LaunchPad to a DRV83xx EVM:
- Connect the three motor phase
terminals to the driver board (phases A, B, and C). If the motor has a center
tap connection or wires for Hall-effect sensors, leave these wires
unconnected.
- Make the inter-device connections
from the MSPM0 LaunchPad kit to the DRV83xx EVM by mating the EVM to the
LaunchPad kit or using jumper wires as shown in Figure 2-4. For hardware user's guide connection details, see Section 2.1.1.
Note: If using the GUI to communicate to the MSPM0 device
using USB to backchannel UART, connect the backchannel UART connections to
UART3_TX and UART3_RX as shown in
Figure 2-5.
- Connect a micro-USB cable from
the MSPM0 LaunchPad kit to the PC.
- Remove GND and 3V3
isolation jumpers on the bridge if desired to isolate the PC from the
motor system. If this step is done, 3V3 must be provided externally or
from the DRV83xx EVM board, if available.
- Supply a voltage compliant with
the Power Supply Voltage (VM) range. For the recommended voltage range, see the
board-specific user's guide or DRV-specific data sheet.
Note: If a different UARTn
port is used to connect the serial pins, configure appropriate UART instance
pins in the SYSCONFIG file of the CCS project.